Technical FAQs

Ask a Question

What is function of control key 1 to 3 of LTMCU when operating mode is reverser in LTMR.

Control key performs below mentioned functions
Operating mode Assignment Key 1 Key 2 Key 3
Reverser 2-wire (maintained) Forward run Reverse run Stop while pressed
3-wire (impulse) Start motor forward Start motor reverse Stop motor
Was this helpful?
What can we do to improve the information ?