Technical FAQs

Ask a Question

Why HMISTO is not able to backup the variable retentive data, alarm log data, and data logging?

Use Run-time Application (Shutdown) operation to backup the variable retentive data, alarm log data, and data logging. If you use other options, these data will be removed.

If you restart the panel with any other options, then the variable retentive data, alarm log data, and data logging will be removed.

Shutdown with Run-time Application (Shutdown) operation to backup these data.

Was this helpful?
What can we do to improve the information ?