Technical FAQs

Ask a Question

Characteristics for Micro SD of M100/M200

Micro SD Card Slot M100/M200

Micro SD Card Slot Characteristics
Topic Characteristics Description
Supported type Standard Capacity Micro SD
High Capacity Micro SDHC
Global memory Size Maximum 32 GB
Speed Classes 4...10
Memory organization Application backup size 64 MB
Data storage size 1.93 GB
Robustness Temperature operating range –25...+85 °C (–13...+185 °F)
Write/erase cycles (typical) See the characteristics provided by your Micro SD card provider for the value.
File retention time
Was this helpful?
What can we do to improve the information ?