Technical FAQs

Ask a Question

What are the measurement accuracy of various parameters like current, voltage, Power ,PF etc. in EM6400NG meter ?

Current,Phase     ±0.5%
Voltage L-N, L-L  ±0.5%
Power Factor        ±0.01
Power                    ±0.5%
Frequency            ±0.05%
Was this helpful?
What can we do to improve the information ?