Technical FAQs

Ask a Question

How to add meter in SBO/EBO.

Follow the below steps to add meter in SBO/EBO:

1. Right click on Enterprise server
2. Click on New > Add Energy folder
3. Right click on Energy folder > New> Site
4. Right clcik on Site>New > Meter
5. Select the type of meter required for configuration .

Also you can refer the attached document file to configure. 
Was this helpful?
What can we do to improve the information ?