Technical FAQs

Ask a Question

Can we upgrade the firmware of 140CRP93•00 and 140CRA93•00 through the 140CRA31908.

It is not possible to use OS Loader / Unity Loader to reach 140CRP93•00 and 140CRA93•00 through the 140CRA31908. 
To update the firmware, it is necessary to keep a Quantum CPU for this operation, or ask Schneider Electric to do so. 
Was this helpful?
What can we do to improve the information ?