Technical FAQs

Ask a Question

How we can generate GSD file of STBNDP2212 module from Advantys configuration Software.

GSD file of STBNDP2212 module can be generated by following below steps:

1. Open Advantys configuration software.
2. Configure the STB island for which GSD is required.
3. Go to File
4. click on Export "Project name"
5. Give the directory path where you want to save the file or keep the default path which is 
6. Click Ok
7. Check for the file on mentioned location.
Was this helpful?
What can we do to improve the information ?