Technical FAQs

Ask a Question

What is the motor voltage range for ATV12H0XXF1 series (1-phase supply voltage 100…120V).

In the ATV12****F1, we have  a voltage doubler integrated in the product, So, the DC bus voltage is the twice of 110 * rootsquare(2),therefore the DC bus voltage is equal to 2 *155.5 = 311VDC (it is the same voltage like the ATV12****M2).It is for this reason that the ATV12****F1 can provide on output 3x220 V.

Was this helpful?
What can we do to improve the information ?