Technical FAQs

Ask a Question

Is the PXP3148MB Modbus Port Expander for the ATS48 Soft Start still available?

Issue:
Is the PXP3148MB Modbus Port Expander for the ATS48 Soft Start still available?

Product Line:
Altistart 48 Soft Starts

Environment:
All

Cause:
Installation

Resolution:
The PXP3148MB Modbus Port Expander is now obsolete and no longer available for purchase. For details on the solution that has replaced this device, please contact MCC tag. 
Was this helpful?
What can we do to improve the information ?