Technical FAQs

Ask a Question

What are the memory types of Sepam 10 & 20 Range.

Sepam 10:
Sepam 10N and Sepam 10B don’t use any batteries. Only Sepam 10A owns a battery (1/2 AA 3.6 V lithium battery) used to back up the internal clock. 
But the events are save in EEPROM and they aren't lost in case power off or reboot. 
 
Sepam 20:
Sepam 20 doesn’t use any battery. Sepam settings are saved in Eeprom memory and disturbance recording data are not saved in case of Power off occurrence.
Was this helpful?
What can we do to improve the information ?