Technical FAQs

Ask a Question

What is the degree of protection of MiCOM P44x relays.

The enclosure protection is as per IEC 60529:
• IP 52 Protection (front panel) against dust and dripping water.
• IP 50 Protection for the rear and sides of the case against dust.
• IP 10 Product safety protection for the rear due to live connections on the terminal block.
Was this helpful?
What can we do to improve the information ?