Technical FAQs

Ask a Question

What is the Ambient Temperature Range of MiCOM P44x relays.

The Ambient Temperature Range of MiCOM P44x relays is as per EN 60068-2-1 & EN / IEC 60068-2-2
Operating temperature range: -25°C to +55°C (or -13°F to +131°F)
Storage and transit: -25°C to +70°C (or -13°F to +158°F)
Was this helpful?
What can we do to improve the information ?