Technical FAQs

Ask a Question

What is the Ambient Humidity Range of MiCOM P44x relays.

The Ambient Humidity Range of MiCOM P44x relays is as 

-> Per EN /IEC 60068-2-78:
    56 days at 93% relative humidity and +40 °C
-> Per EN / IEC 60068-2-14
    5 cycles, -25°C to +55 °C
    1°C / min rate of change
-> Per EN / IEC 60068-2-30
    Damp heat cyclic, six (12 + 12) hour cycles, +25 to +55°C
Was this helpful?
What can we do to improve the information ?