Technical FAQs

Ask a Question

What is the Pollution Degree of MiCOM P44x relays.

The Pollution Degree of MiCOM P44x relays is as per IEC61010-1:1990/A2:1995:
Normally only non-conductive pollution occurs. Occasionally a temporary conductivity caused by condensation must be expected.
Was this helpful?
What can we do to improve the information ?