Technical FAQs

Ask a Question

Do MiCOM P44x relays conforms to corrosive environments.

The MiCOM P44x relays conforms to corrosive environments as per 
-> EN / IEC 60068-2-60, Part 2, Test Ke, Method (class) 3
Industrial corrosive environment/poor environmental control, mixed gas flow test.
21 days at 75% relative humidity and +30°C
Exposure to elevated concentrations of H2S, (100 ppb), NO2, (200 ppb) & Cl2 (20 ppb).

-> EN / IEC 60068-2-52 Salt mist (7 days) 
-> EN / IEC 60068-2-43 for H2S (21 days), 15 ppm
-> EN / IEC 60068-2-42 for SO2 (21 days), 25 ppm
Was this helpful?
What can we do to improve the information ?