Technical FAQs

Ask a Question

What are the Creepage Distances and Clearances of MiCOM P44x relays.

The Creepage Distances and Clearances of MiCOM P44x relays are as per EN / IEC 60255-27: Pollution degree 3, Overvoltage category III.
Was this helpful?
What can we do to improve the information ?