Technical FAQs

Ask a Question

What is the maximum and minimum MMS PDU size for MiCOM P445

        Max MMS PDU size 8000bytes 
        Min MMS PDU size 400bytes
        These data is for P445 having Software Version J7 with Hardware Suffix L along with IEC61850 Edition 1
Was this helpful?
What can we do to improve the information ?