Technical FAQs

Ask a Question

What is the maximum startup time after a power supply interrupt in MiCOM P445

Full IEC61850 services are available after approximate start-up time of 150 seconds. For even big IEC61850 configuration file, time will extend 30 seconds.
These data is for P445 having Software Version J7 with Hardware Suffix L along with IEC61850 Edition 1
Was this helpful?
What can we do to improve the information ?