Technical FAQs

Ask a Question

What is the maximum number of data elements in one data set in MiCOM P445

The maximum number of data elements in one data set in MiCOM P445 is 300
 These data is for P445 having Software Version J7 with Hardware Suffix L along with IEC61850 Edition 1
Was this helpful?
What can we do to improve the information ?