Technical FAQs

Ask a Question

Can the MiCOM P445 server send segmented reports?

Reports will be segmented, and sent with sub-sequence numbers, if the data is too big to fit into a single MMS frame.
These data is for P445 having Software Version J7 with Hardware Suffix L along with IEC61850 Edition 1
Was this helpful?
What can we do to improve the information ?