Technical FAQs

Ask a Question

What is the scan cycle for binary events in reporting model? Is this fixed or configurable in MiCOM P445?

The scan cycle for binary events is 1 ms & it is Fixed.
 These data is for P445 having Software Version J7 with Hardware Suffix L along with IEC61850 Edition 1
Was this helpful?
What can we do to improve the information ?