Technical FAQs

Ask a Question

What is the slow retransmission time in Goose Publishing Model? Is it fixed or configurable in MiCOM P445?

The slow retransmission time in Goose Publishing Model is 60s & it can be configured by GoCB Maximum Cycle Time.
 These data is for P445 having Software Version J7 with Hardware Suffix L along with IEC61850 Edition 1
Was this helpful?
What can we do to improve the information ?