Technical FAQs

Ask a Question

When the time quality bit "Clock not synchronised” set?

The ‘Clock not synchronized’ bit at power-up has a default status of not synchronized (set to one (1)). When the clock becomes synchronized, 
the bit will be reset to zero (0). All available time synchronization sources will affect the ‘Clock not synchronized’ bit. These time sources 
include SNTP and where applicable, IRIG-B.
Was this helpful?
What can we do to improve the information ?