Technical FAQs

Ask a Question

Is there certification and accreditation for PM5110?

Product Line
PM5110

Environment
Certification

Resolution
The PM5110 meter has SGS certification from the external lab.

Refer the attached type test report of PM5110 and  accreditation of SGS lab.

 
Was this helpful?
What can we do to improve the information ?