Technical FAQs

Ask a Question

Does the PM8000 support BACnet protocol?

Product Line
PM8000

Environment
BACnet

Resolution
The PM8000 meters do not support BACnet protocol 

Please refer to page 18 of the following user manual to view the supported protocols:
https://www.schneider-electric.com/en/download/document/7EN02-0336/'

Supported protocols
The meter’s fundamental protocol and architecture is ION.
You can integrate the meter into various industry-standard networks. Data that the meter measures can be made available to other devices using Modbus, DNP 3.0 and SNMP as well as the MV-90 translation system. You can configure the meter to import data from other devices on these networks. The meter supports the IEC 61850 protocol and COMTRADE waveform data format.
The meter also supports IPv6, DPWS and RSTP Ethernet protocols.
 
Was this helpful?
What can we do to improve the information ?