Technical FAQs

Ask a Question

Video:How to select the type of battery to be connected in SRC6KUXI through display?

Kindly follow the below steps: 

1. Press enter key for main menu.
2. Use navigation key to select configuration option.
3.Select battery option under configuration.
4. Press enter key the type of battery will start flashing.
5. Use navigation key to select the battery type as either SMF or Tubular based on battery specs.

Was this helpful?
What can we do to improve the information ?