Technical FAQs

Ask a Question

Can we read Input Status %I , Input Register %IW using IO scanning functionality for Quantum and M340 PLC.

IO scanning is only supports read/write of the holding registers FC03 however to read/write input bit and input register, you can use MBP_MSTR function block for quantum and Read_Var/Write_Var function block for M340 .
 
Was this helpful?
What can we do to improve the information ?