Technical FAQs

Ask a Question

How to connect Delta PLC with HMIGXU3512 using RS-232 in ASCII mode by using Vijeo designer basic software.

In vijeo designer we do not have inbuilt driver for Delta PLCs. 

However there are two protocol variant available in Modbus Protocol as Modbus RTU and Modbus ASCII. In Magelis HMI only Modbus RTU driver is available Modbus ASCII is not supported. 

The best option to communicate is to use protocol converter in between which can convert Modbus ASCII to Modbus RTU or Modbus TCP/IP. 

In Schneider Product basket you can select TSXEGX150 which can convert Modbus ASCII to Modbus TCP/IP but in that case you will have to select HMI having Ethernet port. 
Was this helpful?
What can we do to improve the information ?