Technical FAQs

Ask a Question

“XCSLF3737312” part number will lock actuator when de-energization. what is the part number of this switch with locking on energization and unlocking on de-energization.

 Part number of switch with locking on energization and unlocking on de-energization of the solenoid, replace the 5th number in the selected part number with 5. Example: XCSLF3535312 becomes XCSLF3535512.
So, the part number of switch with locking on energization and unlocking on de-energization will be XCSLF3737512.
 
Was this helpful?
What can we do to improve the information ?