Technical FAQs

Ask a Question

Is it possible to test and run the ATV630 drive without motor.

Yes, it is possible. 
 program - [OutPhaseLoss Assign] OPL to [Function Inactive] 

And other programming parameters will remain same. 
Was this helpful?
What can we do to improve the information ?