Technical FAQs

Ask a Question

What is the speed range for ATV340 drives.

Following are the Speed Range for ATV340.
1-100 in open loop Asynchronous law   
1-50 in open loop Synchronous law                                                                                            
1-1000 in closed loop.
   
Example; For a 50Hz motor:
Speed range 1-100 means the drive is able to give the nominal torque between 0.5Hz to 50Hz.
Speed range 1-50 means the drive is able to give the nominal torque between 1Hz to 50Hz.
Speed range 1-1000 means the drive is able to give the nominal torque between 0.05Hz to 50Hz.

 
Was this helpful?
What can we do to improve the information ?