Technical FAQs

Ask a Question

Is possible to get ISO 9001 certificate of RXM4AB1P7.

RXM4AB1P7 is manufactured in Batam, Indonesia.
So, Refer ISO certificate of Batam plant in attachment.
Note: There is no ISO 9001 certificate of RXM4AB1P7 product. Only manufacturing plant are ISO 9001 certified.
Was this helpful?
What can we do to improve the information ?