Technical FAQs

Ask a Question

Is it possible to continue operation if there is no Analog Input signal (4 to 20 mA) on ATV630 drives.

=Yes, it is possible.
=>Program LFL1 to [Spd maint.] rLS
=> The drive maintains the speed being applied when the detected error occurred, as long as the detected error is active and the run command has not been removed. Refer to attached page from programming manual.

 
Was this helpful?
What can we do to improve the information ?