Technical FAQs

Ask a Question

What is the current transformer(CT) characteristic for Accusine PCS+.

Please find below specification of current transformer(CT) characteristic for Accusine PCS+:
  • Any ratio with 1 or 5 ampere secondary
  • Type 1 accuracy
  • 50/60 or 400 Hz rated (Instrument rated or better)
  • Grounded
  • Can be shared with other devices
Was this helpful?
What can we do to improve the information ?