Technical FAQs

Ask a Question

What is the operating Contaminant Levels of Accusine PCS+.

The operating Contaminant Levels as per IEC60721-3-3 of Accusine PCS+ is as follows:
  • Chemical Class 3C2
  • Mechanical Class 3S2
  • No conductive particles permitted
Was this helpful?
What can we do to improve the information ?