Technical FAQs

Ask a Question

What is the part number of HMI which can be used with XUW vision sensor to view the objects.

For this type of application; it is not possible to use a standard HMI, you need to use an HMI with windows embedded (ex: HMIG5U+HMIDT542), because of the XUW vision sensor software is needed in order to visualized the picture on the HMI .
Was this helpful?
What can we do to improve the information ?