Technical FAQs

Ask a Question

Is it possible to upgrade Automation Server (AS) from 1.9.1 to 1.9.2 ?

Yes we can upgrade to 1.9.2 but for that we only need the 1.9.2 device administrator hotfix, not the full install setup.
Was this helpful?
What can we do to improve the information ?