Technical FAQs

Ask a Question

On ATV312 Analog Input AI1 (0 – 10V) ; which value corresponds to 10V.

10 V corresponds to HSP.
If HSP = 50 Hz
For Example: AI1 receives 0 ~ 10V and operates at 0 ~ 50Hz.
If 5V is input, it will operate at 25Hz.

Was this helpful?
What can we do to improve the information ?