Technical FAQs

Ask a Question

Do we have finger scanners that can be connected to a HMI.

The USB Biometric Switches communicate with the PC/HMI via the USB port to manage the
user database. This database can be visualized, saved, and duplicated by PC/HMI
with XB5S Soft application (1) (2). The fingerprint records can also be erased in the
absence of users. The Schneider HMI (3) with Vijeo Designer software (4) enables the switches to
authorize different access levels and trace HMI operations of each use.
(1) =>Compatible with all versions of Harmony XB5S Soft application. The XB5S Soft is a freeware
application and can be downloaded from our website
(2) =>The user database cannot be uploaded from USB biometric switch to the PC.
(3)=> Compatible with Magelis iPC, STU, OT, GXO, GT (except GT1000 series), GK, GH, and
GTO models .
(4)=> Compatible with VijeoDesigner HMI editor software V6.1, Service pack 2.
Was this helpful?
What can we do to improve the information ?