Technical FAQs

Ask a Question

How to program ATV630 for quick /immediate stop for the system.

First program the [Dec.Ramp Adapt] brA to No.
First Method:-
=>You should select the ramp stop and set the minimum ramp time for decceleration (parameter DEC ), as this value : 0.1s (you can program DEC as per the requirement)
Then you will be able to stop with a time near 100ms, depending on the torque and current limitation.
 Second Method:-
=>program [Type of stop] Stt to [DC injection] and program parameters related to DC injection as per the requirement.

Was this helpful?
What can we do to improve the information ?