Technical FAQs

Ask a Question

What are the causes of PTC fault on ATV71 drive.

PTC fault comes when:--
(1) PTC resistance is below 50 ohms
(2) PTC is open circuit
 
=>check PTC resistance value
=>check it by replacing the PTC
Was this helpful?
What can we do to improve the information ?