Technical FAQs

Ask a Question

What are the Building Standards which an AS-P supports.

AS-P natively communicates with three of the most popular communication protocols:

  • BACnet: AS-P directly communicates to BACnet/IP and BACnet MS/TP networks, which provides access to b3 devices and BACnet devices.

  • LonWorks: AS-P has a built-in FTT-10 port, which enables access to Xenta devices and LonWorks devices.

  • Modbus: AS-P natively integrates Modbus RS-485 master and slave configurations, as well as IP client and server. This integration provides access to devices that communicate on the Modbus protocol, such as power meters, circuit breakers, and lighting controllers.

Was this helpful?
What can we do to improve the information ?