Technical FAQs

Ask a Question

What is the type of memory which an AS-P has.

AS-P has two types of memory:

  • 512 MB DDR3 SDRAM (for program execution)

  • 4 GB eMMC memory (for storage)

If a power failure occurs, all important variables are automatically saved to the eMMC memory before complete shutdown. When power returns, this data retention function ensures that AS-P can continue to run with the correct set of values.

Was this helpful?
What can we do to improve the information ?