Technical FAQs

Ask a Question

How to configure the SmartStruxure server device IP address (AS-P/AS-B).

  1. In Device Administrator, select the SmartStruxure server device for which you want to configure an IP address.

  2. On the View menu, click Network settings .

  3. Clear Enable DHCP .

  4. In the Host name box, type a unique host name for the SmartStruxure server device.

  5. In the Domain box, type the name of the domain.

  6. In the Static IP address box, type an IP address for the SmartStruxure server device.

  7. In the Netmask box, type the prefix of the subnet.

  8. In the Gateway box, type the address to the router.

  9. In the Primary DNS box, type the address to the primary DNS server.

  10. In the Secondary DNS box, type the address to the secondary DNS server.

  11. In the Tertiary DNS box, type the address to the tertiary DNS server.

  12. Click OK .

  13. In the IP changes dialog box, click OK .

Was this helpful?
What can we do to improve the information ?