Technical FAQs

Ask a Question

Is it possible to connect HART analog sensors to TM3 family analog module

HART sensors can be connected to TM3 analog modules but then only analog signal (4-20 mA) can be received, as TM3AI8 has no HART capabilities.
Unfortunately none of the TM2 / TM3 / TM5 modules can do HART.
Was this helpful?
What can we do to improve the information ?