Technical FAQs

Ask a Question

Is it possible to open multiple instances of somove software

Yes it is possible to open more than one instance of SoMove software. This feature introduced with SoMove FDT ( Field Device Tool) version v2.5.
SoMove FDT versions v2.5 and onwards it is possible to open more than one instance of SoMove software.
Was this helpful?
What can we do to improve the information ?