Technical FAQs

Ask a Question

Is zelio smart relay support PID function block

yes, Zelio soft version v5.0 evolved with new function block of PID control. User should use zelio soft2 v5.0 and upgrade the zelio smart
relay with firmware version equivalent of zelio soft2 v5.0 to use PID. User should select FBD language to use PID.
This feature is available for zelio soft v5.0 and onwards releases.
Was this helpful?
What can we do to improve the information ?