Technical FAQs

Ask a Question

What is the maximum nos. of variables that can be shared over OPC UA server connection in M241 / M251

 Maximum nos. of 1000 variables in cycle time 200 ms can be shared over OPC UA server connection on M241 / M251 controller.
Was this helpful?
What can we do to improve the information ?