Technical FAQs

Ask a Question

Relay R3 configured to tAI; When Relay R3 will be activated on ATS48 Soft Starter.

When you configure R3 = tAI (Motor Thermal Alarm): this relay will be activated when the tHr (motor thermal state) is > 110%. in this case ATS48 will not trip in fault. the state of R3 will be deactivated if tHr <110%.
Note:  A thermal fault stops the motor if it exceeds the critical temperature rise threshold (motor thermal state >125%).
Was this helpful?
What can we do to improve the information ?