Technical FAQs

Ask a Question

LXM28 fault AL5A1 and Wn720

Issue:
LXM28 fault AL5A1

Product Line:
LXM28
Lexium 28 all part numbers

Resolution:

AL5A1 and Wn720 are two faults that remain after the production process. This is a known issue that was already fixed and new drives are now manufactured without this fault. The way of removing these two faults is by resetting the drive to factory settings via P2-08=10. No need to re-flash the firmware.
Was this helpful?
What can we do to improve the information ?